AXIS#.UNIT.PLINEAR

Description

AXIS#.UNIT.PLINEAR sets the units type for the position parameters when the motor type (AXIS#.MOTOR.TYPE) is linear.

Type

Description

0

counts

1

Millimeters (mm)

2

Micrometers (µm)

3

Custom Units (PIN/POUT) per revolution

4

counts 16-bit

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 4

Default Value

1

Data Type

Integer

See Also

AXIS#.PL.FB, AXIS#.PL.CMD, AXIS#.MOTOR.TYPE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.UNIT.PLINEAR

5010h

07h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6603

1

6603 (0x19cb)

AXIS1.UNIT.PLINEAR

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.UNIT.PLINEAR

6603

Unsigned8

Read/Write

-